Article
Intelligent air venting
Air is one of the most common faults found in heating systems.
How can you detect and eliminate the problem before it’s too late? The new ALPHA includes a tool to detect air in the system and and initiate an automatic venting process.
Watch video to learn more
Connect to the pump using the Grundfos GO app and configure the air venting procedure after commissioning or during operations. When air passes through the pump, the ALPHA will detect it and automatically initiate an air venting procedure. This triggers a notification in the Grundfos GO app, serving as a reliable tool to identify faults in the heating system and ensure comfort for homeowners.
Explore all the features of the digital ALPHA
The ALPHA pump unlocks a world of new opportunities for data-driven insights for easier troubleshooting. Discover, analyze, and respond in real-time with an intelligent pump designed for the modern era. With smarter, more detailed data, you can be ready for whatever comes next.
Step into the future with the right pump
ALPHA
ALPHA is a connected and fully digital pump that offers troubleshooting. Commission automatically with a pump made for both existing and future domestic heating systems – ensuring you are prepared for whatever comes next.
UPSe
Demand for more energy-efficient and sustainable heating systems is on the rise. An inefficient circulator is not the place to waste energy. Powered by electronically commutated motors (ECM) technology, the UPSe pump features dry-run protection, improved wiring for easier installation with a toolless power connector, and automatic self-venting – making it the most efficient pump on the market.