Article

Minimize pump installation time and troubleshoot with confidence

It’s time to take the guesswork out of residential heating system repairs. With Grundfos Digital NEXT you get faster troubleshooting, faster pump replacement, faster installation, and faster commissioning.

Watch video to learn more

Eliminate wasted time

Moving from troubleshooting and pump replacement to installation and commissioning can be a time-consuming process – and then there is the risk of call-backs when the selected pump doesn’t fit the application.

Grundfos offerings eliminate wasted time.

Once your Grundfos pump is installed, log in to the Grundfos GO app, which will guide you through the setup process. The benefits of guided commissioning don't stop there. Homeowners will automatically save 25% electricity compared to simply setting the pump to setting III.

Once setup is complete and the pump is wired with the easy and accessible power connector, simply initiate the air venting sequence with the Grundfos GO app. The pulsating venting sequence will push air to the air vent quickly while at the same time allowing the air to escape into the air vent.

If you’re not sure which pump to select when replacing a broken pump, you can also use the Grundfos GO app's replacement procedure, which provides an optimal recommendation. ALPHA can replace more than 90% of small circulators on the market.

Step into the future with the right pump

ALPHA

ALPHA is a  fully digital pump that offers Bluetooth connectivity and a touch-screen interface, intelligent troubleshooting, improved AUTOADAPT, and automated firmware updates.  Commission automatically with a pump made to adapt to existing and future domestic heating systems – ensuring you are prepared for whatever comes next.

UPSe

The demand for more energy-efficient and sustainable heating systems is on the rise. An inefficient circulator is not the place to waste energy. Powered by electronically commutated motors (ECM) technology, the UPSe pump features robust startup, dry-run protection, improved wiring with a toolless power connector, and a best-in-class Hydraulic Institute Energy Rating in the market– making it the most efficient pump in the small circulator space.

Explore all the features of the digital ALPHA

The ALPHA pump unlocks a world of new opportunities for data-driven insights for easier troubleshooting. Discover, analyze, and respond in real-time with an intelligent pump designed for the modern era. With smarter, more detailed data, you can be ready for whatever comes next.


With the new ALPHA, you get built-in technology that allows you to easily troubleshoot…
 


Powered by electronically commutated motors (ECM) Grundfos circulators features the highest Hydraulic Institute Energy Rating in the market.
 


With the new ALPHA, you get a digital solution that ensures you’re always on top of the latest developments…


To avoid unwanted noise and reduced performance Grundfos pumps are self-venting in any setting and mode.
 


With the new ALPHA, you get guided setup, which gives you recommendation and ensures optimal performance.


With the new ALPHA, you get comparable replacement recommendations using the Grundfos GO app to replace a variety of different Grundfos and competitor products.…

Be ready for whatever comes next

Sign up for our newsletter to stay up-to-date on Digital NEXT news and announcements. We’ll keep you in the loop of all our digital developments so you can be ready for what comes next.