Meet the expert
A smarter way to reduce pressure fluctuations
When does water hammer become an issue for a submersible pumping installation? We often hear that question, and the general rule is that this can be the case when you have relatively long discharge pipelines with a relatively small pipe diameter. Soft starting and stopping of the pump do not necessarily resolve the problem, which arise when accelerating and decelerating the water mass in the pipes. We need to do more, for example by placing a membrane tank after the pump well head.
However, the best solution is to add a Variable Frequency Drive (VFD) as well. The video explains why this is a smarter way reducing the pressure fluctuations that can cause water hammer in submersible pumping installations.
Other related articles and insights
Find related articles with research and insights from Grundfos.
Related applications
Find applications from Grundfos related to this subject.
Related products
Find products from Grundfos related to this subject.