News
Fire protection matters with Grundfos
06-May-2019
As you would expect, safety was an important factor that was integrated into every aspect and Grundfos Pumps were delighted to be involved with assisting in specifying and supplying a specialist pre-fabricated school pump house. The OH1-15 single electric packaged pump house is fully compliant with all standards and technical bulletins. With a compact footprint of just 2m x 2.5m these units arrive on site fully commissioned and ready to plug n’ pump.
Fire safety is something very much in focus these days and Grundfos are ideally positioned to meet a wide range of fire requirements from compact domestic units, through ordinary and high hazard sets, FM/UL sets as well as a wide range of hydrants and wet risers. All fire sets are built in the UK and deliver a robust and cost-effective solution.
This new campus was built to meet a range of needs and is set to play a central role, not only in education but also in the wider community and Grundfos Pumps are pleased to be delivering the fire related peace of mind.