Case

Park Plaza opens right on time

Park Plaza hotels have gained an enviable reputation for providing guests with a range of excellent facilities, and for their prime locations around the world. The latest edition to the Plaza family and their 6th hotel in London certainly lives up to this promise.

Built on the site of what was formerly the County Hall Annexe and at a cost of £350m, The Park Plaza Westminster Bridge offers 1,021 rooms that range from penthouses and studios, to well appointed guest rooms, as well as providing a wide range of amenities and facilities. The hotel is also set to become a business meeting hub with a huge 2,700 square metres of flexible meeting space spread across 3 floors. This includes the Westminster Ballroom that can accommodate 1,400 theatre style or 1,000 for dinner.  All this means that, this new kid in town is one the largest hotel developments in Europe.

Meeting the exacting standards expected from the great diversity of visitors and guests, is a complete turnkey solution of energy efficient Grundfos pumps. Included in the line-up are a wide range of circulator and centrifugal pumps that support heating and hot water services as well as cooling and air-conditioning needs, single stage standard pumps for liquid transfer, and Grundfos Hydro MPCE booster sets that will deliver the required amounts of water, to where it is needed, the system is also supported by a range of SEV sewage pumps. Grundfos fire sets offer that extra level of assurance that will ensure a good nights sleep.

This hotel will certainly be noticed as its excellent position means it offers uninterrupted views across the Thames to Big Ben and the Houses of Parliament and it is only few minutes stroll from the London Eye. With such illustrious neighbours and with a unique architectural style this new hotel is sure to become a firm favourite and the complete Grundfos pump solution will play its role in ensuring that the delivery will match the promise all day, every day.