8 otázek Pokročilý

Ecademy test

29 - Introduction to temperature control

Tento test obsahuje 8 Může být kdykoliv opakován.

Ke splnění testu musíte odpovědět správně všechny otázky.

Začít test

Otázka 4 z 8 Pokročilý

How high is the suction lift of the self-priming CM pump?

Otázka 5 z 8 Pokročilý

What is the expected payback time of an investment in system optimisation?

Otázka 6 z 8 Pokročilý

What is the ratio between the capital investment and running costs of a temperature control system?

Otázka 7 z 8 Pokročilý

How do you prevent pumps from malfunctioning when transporting hot water with a temperature of well above 120C°?

Otázka 8 z 8 Pokročilý

Spokojeni se svými odpověďmi?

Potvrďte odpovědi a přejděte k vyhodnocení testu.

Vyhodnotit

Výsledek testu

Gratulujeme, splnili jste test 29 - Introduction to temperature control

Získané odznaky:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Pokračovat Přejít do MyEcademy

Bohužel. Tentokrát jste 29 - Introduction to temperature control neprošel testem.

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: What is the most efficient and simple way of controlling heating, cooling and refrigeration systems?
A: Intelligent pumps equipped with temperature sensors that measure the outlet temperature and signal the pump to regulate its flow accordingly – without the use of valves.
Correct
Q: Which load profile will benefit the most from a demand driven control system?
A: Low flow rate with relatively few peak periods during the day.
Correct
Q: Why is ammonia an efficient coolant?
A: Ammonia is able to absorb large amount of heat when it evaporates.
Correct
Q: How high is the suction lift of the self-priming CM pump?
A: Up to 8 metres
Correct
Q: What is the expected payback time of an investment in system optimisation?
A: 1-5 years
Correct
Q: What is the ratio between the capital investment and running costs of a temperature control system?
A: 1:20
Correct
Q: How do you prevent pumps from malfunctioning when transporting hot water with a temperature of well above 120C°?
A: Equip the pump with double-shaft seals or air-cooled top.
Correct
Q: Which temperature control systems hold the greatest potential for optimisation?
A: Three way valve Regulated temperature control systems that adapts operation according to the load.