FAQ
Question: The pump is making loud noises. What should I do?
Answer:
Loud noises can be due to trapped air in the system or a mechanical issue. If the issue doesn't resolve after the system is fully filled with water, contact a professional.
Additional information:
Get to know more about the product range or see more on SCALA1 or SCALA2.