FAQ

Question: How does a lifting station work?

Answer:

What is a Grundfos SOLOLIFT2 and how does it work? 

Grundfos SOLOLIFT2 is a compact wastewater lifting stations that efficiently handles wastewater and sewage from various sources like toilets, showers, sinks, washing machines, and dishwashers. SOLOLIFT2 transports the wastewater to either the main sewage system or an elevated drainage point. Making it possible to place sanitary appliances without worrying about the location of the existing gravity drainpipe.

What types of wastewater and sewage can be handled by Grundfos SOLOLIFT2? 

The 5 variants of SOLOLIFT2 can effectively handle different types of wastewater and sewage, including those originating from toilets, showers, sinks, washing machines, dishwashers, as well as condensate from boilers and air conditioning units. Both black and grey wastewater from the home. The specific models within the SOLOLIFT2 range have different capabilities and capacity. Therefore, it is important to choose the appropriate model based on the specific requirements of your wastewater and sewage needs.

Use this guide to make selection easier.

Can Grundfos SOLOLIFT2 handle both residential and commercial applications? 

A SOLOLIFT2 can handle wastewater from 1 toilet only and 1 to 3 other appliances. For larger commercial buildings we have the MULTILIFT Range. 

Are there any environmental or safety concerns to consider when using Grundfos SOLOLIFT2, and how can I ensure that it is being used properly and responsibly? 

As an installer, it is crucial to prioritize environmental and safety considerations when working with Grundfos SOLOLIFT2. Adhere to local regulations and guidelines concerning the handling and disposal of wastewater and sewage. Proper installation is essential, ensuring compliance.

Additional information:

Get to know more about the product range. The model or find specific documentation.

The SOLOLIFT2 Lifting station course – get an introduction to our range in our Ecademy. It is a free online training tool.