FAQ
Question: How are the Grundfos Machine Health sensors installed?
Answer:
Grundfos Machine Health is non-invasive and non-intrusively installed. Sensors are mounted using epoxy glue.
Additional information:
Immediate, predictive insights allow you to pinpoint problems before they become costly failures. With Grundfos Machine Health, you can reduce unexpected mechanical breakdowns by up to 75%.