Dairies
1 - The first step is to lower carbon emissions in operations by 63% at 60 dairies worldwide by 2030
Source: Arla.com
2 - 481,800 kWh energy savings in critical water supply systems at Arla’s Westbury site in the UK
Source: Arla Westbury, case story
Soft Drinks
1 - The global demand for fresh water is expected to outpace its supply by 40% before 2030.
Source: Water Scarcity: A Growing Investment Concern, Morgan Stanley
Breweries
1 - The brewing industry is one of the largest industrial users of water.
Source: The brewing industry and environmental challenges
2 - 70% of the fresh water used in brewing ends up as wastewater.
Source: Reducing Water and Wastewater in the Brewing Industry
Meat & Poultry
1 - Pumps account for as much as 40% of industrial energy use.
Source: 5 ways pumps can help power your sustainability transformation