8 Vragen Gemiddeld

ECADEMY test

3 - Afvalwater in gebouwen

Deze cursustoets bevat 8 vragen. Opnieuw beantwoorden kan altijd..

Alle vragen moeten correct zijn beantwoord om te slagen voor de test en de cursus te voltooien..

Begin test

Vraag 3 van 8 Gemiddeld

Which method of backflow prevention has the following disadvantages: Highly sensitive to sand and solid objects in the water. In a backflow situation, it is not possible to use the sanitary facilities that are connected to this device. Storm water drains cannot be connected to this device. The device is not 100% safe and should be used only to protect secondary rooms with no vital technical installations.

Vraag 4 van 8 Gemiddeld

Which method of backflow prevention has the following advantages: Offers maximum backflow and flooding protection: Is not sensitive to fat, grease, sands and solids in the water. Makes it possible to use sanitary facilities in case of backflow. Offers protection for paved areas. Can be connected to buildings’ storm water drains.

Vraag 8 van 8 Gemiddeld

Tevreden met uw antwoorden?

Vul jouw huidige antwoorden in en ontvang het definitieve testresultaat.

Indienen

Resultaten van de test

Gefeliciteerd. U bent geslaagd voor de test en heeft de cursus voltooid 3 - Afvalwater in gebouwen

Behaalde badges:

Wat voor beoordeling geeft u deze cursus?

U kunt een beoordeling aan deze cursus toevoegen. Vergeet niet dat u ingelogd moet zijn voordat u de toets doet om uw beoordeling te kunnen geven.

Ga door met trainen Ga naar MyECADEMY

Sorry. U heeft het niet gehaald 3 - Afvalwater in gebouwen Test deze keer

Wat voor beoordeling geeft u deze cursus?

U kunt een beoordeling aan deze cursus toevoegen. Vergeet niet dat u ingelogd moet zijn voordat u de toets doet om uw beoordeling te kunnen geven.

Correct
Q: What are the disadvantages of the traditional gravitation system?
A: Many gravitation pipes have to be installed outside the building and a great deal of excavation work is needed.
Correct
Q: Under which circumstances should you consider a pressurised wastewater system rather than a gravitation system
A: When there is a long distance between the building and the sewer main, when the sewer main is up-hill or when there are obstacles between the building and the sewer main.
Correct
Q: Which method of backflow prevention has the following disadvantages: Highly sensitive to sand and solid objects in the water. In a backflow situation, it is not possible to use the sanitary facilities that are connected to this device. Storm water drains cannot be connected to this device. The device is not 100% safe and should be used only to protect secondary rooms with no vital technical installations.
A: Anti-flooding valves
Correct
Q: Which method of backflow prevention has the following advantages: Offers maximum backflow and flooding protection: Is not sensitive to fat, grease, sands and solids in the water. Makes it possible to use sanitary facilities in case of backflow. Offers protection for paved areas. Can be connected to buildings’ storm water drains.
A: Pumping stations
Correct
Q: Why is the life cycle cost of the pressurised wastewater system low?
A: The initial cost of the lifting station is lower compared with a pit and there are no gravitation pipes outside the building
Correct
Q: What are the four most common types of wastewater from commercial buildings?
A: Wastewater, storm water, drainage water and wastewater from parking areas
Correct
Q: What is grey wastewater?
A: Water, which is discharged from showers, sinks, washing machines, canteen kitchens etc.
Correct
Q: Of the three anti-flooding systems, why is the lifting station the superior system?
A: It is pre-assembled and its location inside the building makes it easily accessible for service. Furthermore, it offers maximum backflow and flooding protection