The new generation Grundfos CR pumps are designed for world-class efficiency and reliability - with millions of customisable solutions.
The CR 255 pump completes the CR range and continues to push the boundaries
The impressive new CR 255 is now available, completing the CR range and continuing to move limits with a flow range up to 320m3/h.
After the last big addition of the CR 185 and CR 215 pumps – with a flow range capacity up to 240 m3/h and 280m3/h respectively – we continue to push the boundaries with this strong addition to the world’s most modular pump range. Our new hydraulic design improves everything from impeller and guide vanes to inlet, discharge port, sleeve and diffuser – giving you world-class energy efficiency and improving pump reliability even more than before.
Our CR range delivers world-class reliability, with pumps that are tested to the absolute limits and beyond to offer optimised operating economy via enhanced hydraulic efficiency. The CR pump range provides literally millions of solutions to fit your every application need.
The CR 255, CR 215 and CR 185 are three new CR pumps that together with the CR range continue to push the boundaries of performance. Find out more below and get a first-hand look at the added value of the new flow range capacities brought to you by the CR 255, CR 215 and CR 185. The pumps have been designed using state-of-the-art simulation-driven processes and have been field-tested around the world – so you can install and operate the range with total confidence.
Going beyond expectations to meet water challenges
Our extra-large CR pumps are not alone in going beyond expectations to meet the challenges of water. Joana Andrade does this too, competing in the extreme sport of big wave surfing. Find out how our shared passion for the flow of water inspire Joana and Grundfos – and how we, each in our own way, move the limits beyond the expected.
A tradition of excellence: follow the CR through five decades
It all started with a request from a customer in 1971. That was when Grundfos invented the vertical, multistage, centrifugal in-line pump concept. Watch our film about the development of the CR pump through five decades, told by the Grundfos specialists who were there at each step of the journey.
Let’s meet and talk more about how the CR pump range helps you
Want to meet and talk more about how Grundfos can help you match a CR pump to your demanding application? Let’s discuss how you can maximise your investment and get the most from the new extended range of CR pumps.
How can we help you?
Whether you’re looking to buy a product or simply seeking advice from a Grundfos expert, we are more than happy to help you get the most out of your pump solution! Feel free to get in touch if you need support.
Related applications
Find applications from Grundfos related to this subject.
Explore the full CR pump range in detail
The new generation of Grundfos CR pumps introduces world-class ef-ficiency upgrades and a range of new features that will further improve pump reliability.
CR Showroom
Enter the world of the new generation CR!
The showroom is where you get a 360° view of CR multistage inline pumps.
Much of a pressure-boosting pump’s total cost goes to energy and maintenance. Read the Grundfos whitepaper to increase your understanding of how you get better results from an investment in pressure-boosting performance.
Increased efficiency and reduced downtime at a chemical plant
A chemical plant in mid-west USA required a reliable pump to match the demands of chemical production. Here, a CR 95 pumps were installed, increasing efficiency and reducing downtime at the plant. In fact, the pumps proved to be almost maintenance free.
Large savings and efficiency gains for a water utility
In Austria, a water utility installed a Grundfos CR 95 pump from the new extended range to ensure a safe, energy-efficient and cost-saving water supply to 50,000 residents. In addition, the new pump fits with the utility’s own sustainability ambitions.
Let’s meet and talk more about how the CR pump range helps you
Please, fill out the form below and one of our Grundfos specialists will get back to you.
Thank you for your request! We will get back to you as soon as possible.
Keep an eye on your inbox, a confirmation email is coming your way!
Click the link in the email to complete the subscription process and you’ll start receiving all the most relevant news and updates from Grundfos. If you don’t complete the sign-up process, you won’t be able to receive our newsletter.
If you’re already subscribed, you will not receive the confirmation email.
Kind regards
Grundfos