6 questions Intermediate

ECADEMY test

64 - ALPHA HWR and ALPHA COMFORT SYSTEM range

This course test contains 6 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 1 of 6 Intermediate

What type of hot water recirculation system is the ALPHA HWR designed for?

Question 2 of 6 Intermediate

How do you remedy the pump blocked alarm on the ALPHA HWR and ALPHA COMFORT SYSTEM pumps?

Question 3 of 6 Intermediate

How do you identify a dry run alarm on both the ALPHA HWR and ALPHA COMFORT SYSTEM pumps?

Question 4 of 6 Intermediate

What potential issues may arise if the incorrect speed setting is chosen during the setup of the ALPHA HWR or ALPHA COMFORT SYSTEM pumps?

Question 5 of 6 Intermediate

What are the two states involved in the process where the ALPHA COMFORT SYSTEM learns when the comfort valve is closed?

Question 6 of 6 Intermediate

Which control mode for the ALPHA HWR operates on a constant curve and has three different settings labelled I, II, and III?

Question 6 of 6 Intermediate

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 64 - ALPHA HWR and ALPHA COMFORT SYSTEM range

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 64 - ALPHA HWR and ALPHA COMFORT SYSTEM range test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: What type of hot water recirculation system is the ALPHA HWR designed for?
A: Systems with a dedicated return line
Correct
Q: How do you remedy the pump blocked alarm on the ALPHA HWR and ALPHA COMFORT SYSTEM pumps?
A: Check the system for impurities and remove any found
Correct
Q: How do you identify a dry run alarm on both the ALPHA HWR and ALPHA COMFORT SYSTEM pumps?
A: Two blinking red eye lights
Correct
Q: What potential issues may arise if the incorrect speed setting is chosen during the setup of the ALPHA HWR or ALPHA COMFORT SYSTEM pumps?
A: Excessive energy consumption, noise in the system, and resident discomfort
Correct
Q: What are the two states involved in the process where the ALPHA COMFORT SYSTEM learns when the comfort valve is closed?
A: Learning State and Operating State
Correct
Q: Which control mode for the ALPHA HWR operates on a constant curve and has three different settings labelled I, II, and III?
A: 24/7 mode