Case
Medical cooling by Beehe with Grundfos Direct Sensors™
The Company
Shanghai Beehe Electric Co. Ltd is a major cooling system supplier for global medical imaging companies. Production is based primarily in China. Since 2014, Beehe has supplied more than 1,000 units to OEM customers. Beehe delivers the critical cooling for customers' MRI, PET and PET-MR modules.
The Situation
To measure the flow rate of different cooling loops in Magnetic Resonance Cooling System Beehe needed a flow sensor with high accuracy, low cost, small size, analogue output and without moving parts inside. Grundfos VFS series flow sensors combines all the requirements described above, so Grundfos was chosen at the beginning of selection.
The Grundfos Solution
VFS 10-200 were delivered and were installed in the different cooling loops for Magnetic Resonance Cooling System. As this application needs higher accuracy in the low flow area, now the new improved VFS version with better low flow performance is delivered to Beehe.
The Outcome
VFS sensors are 2 in 1 sensors, where flow and temperature measurement functions are integrated. With this temperature measurement, Beehe can use the T signal to evaluate the temperature level in the different loops. But the T accuracy of VFS is ±1 and 2℃ (0-100℃), which is not enough to use this T signal to control the cooling system. So, if this T accuracy can be improved to ±0.5℃(0-100℃), then Beehe can use it to control the system. This is a point where Grundfos is working to deliver higher accuracy sensors in the near future.
Grundfos VFS sensors supplies us a higher accuracy, lower cost flowsensor solution which increased our competitiveness compared with other competitors in the medical cooling area. At the same time, the VFS series are very easy to use and high quality in the long life time.