FAQ
Question: How do I install the underwater cable for submersibles?
Answer:
Before installing the underwater cable on the motor, you need to make sure that the cable plug is clean and dry. For ease of installation, the rubber parts of the cable plug should be coated with a non-conductive silicone paste. The screws that hold the cable in place should be tightened using the following tightening torques:
MS 4000: 2.0 Nm
MS 402: 2.0 Nm
MS 6000: 4.0-5.0 Nm
MMS 6000: 10 Nm
MMS 12000: 15 Nm
Additional information:
Enhance your knowledge
Find out how to get reduced energy consumption, increased comfort and unsurpassed operational reliability for your application. Read our customers' stories to learn how they benefit from the Grundfos approach to intelligence, water and energy. You can also search Grundfos research and insights for more learning materials, articles, white papers, videos and much more content to inform your solution.