FAQ

Question: How are the Grundfos Machine Health sensors installed?

Answer:

Grundfos Machine Health is non-invasive and non-intrusively installed. Sensors are mounted using epoxy glue.

Additional information:

Immediate, predictive insights allow you to pinpoint problems before they become costly failures. With Grundfos Machine Health, you can reduce unexpected mechanical breakdowns by up to 75%.