FAQ
Question: Can Grundfos Machine Health accurately diagnose a machine if the machine is old and already has problems?
Answer:
Yes, our Machine Learning algorithms will take up to 2-3 weeks baseline process when first installed on your machines, but the data we collect is sufficient to identify faults on both new or old machines that may have existing issues. In fact, 40% of the machines we diagnose have some sort of issue identified upon exiting baseline.
Additional information:
Immediate, predictive insights allow you to pinpoint problems before they become costly failures. With Grundfos Machine Health, you can reduce unexpected mechanical breakdowns by up to 75%.