See how it's done

Cooling towers and chillers are responsible for as much as 70% of the water used at an industrial facility. Many of these systems are operating less than optimally – some using as much as 50% more water than necessary. Saving water means saving money. Not only on bills for potable water, but on wastewater, chemical treatment, and energy.

Let our expert show you how to optimize your cooling system through pumps, controls and system intelligence.

Request a virtual energy savings consultation

With four simple data points (flow, head, efficiency and annual run hours), we will calculate how much Grundfos' intelligent solutions can save you.

Increasing efficiency and reducing waste has never been simpler than with a complete industrial cooling bundle from Grundfos

Each Grundfos iSolutions for Cooling Towers bundle includes the following pre-configured components:

  • Two end-suction pumps – duty/standby (LCS or LCSE)
  • Two variable-speed drives (external or pump integrated)
  • Two pressure and temperature sensors (RPI+T)
  • One Multi-Pump Control (MPC) panel

Take Control and Maximize Industrial Cooling Efficiency

Pumps play a large role in cooling systems. Read about the areas where pumps impact performance and the benefits of integrating intelligent, variable speed pumping solutions.

Annual Savings of $245,000

Read about how Grundfos delivered significant energy savings and system optimizations for a leading engine and turbine manufacturer.

More than 70% energy savings

Read about how a major US Adhesive manufacturing company has been able to optimize performance and achieve significant OPEX savings.

Related products

Find products from Grundfos related to this subject.