FAQ

Question: What minimum fill level is required to properly operate the wastewater or deainage pump?

Answer:

The EF and SE pumps are equipped with motors cooled by the surrounding pumped medium. In order for the motors to be adequately cooled, the EF and SE pumps must always be completely submerged in the pumped medium during operation. For applications where this is not possible, the fill level must never fall below half the height of the pump.

The KP and AP pumps, on the other hand, have motors that are cooled from the inside by the pumped medium flowing through the pump. For this reason, during operation these pumps need not be submerged in the pumped medium, such that shallow pumping down to a level of 3 cm is possible.

Additional information:

Enhance your knowledge

Find out how to get reduced energy consumption, increased comfort and unsurpassed operational reliability for your application. Read our customers' stories about how they benefit from the Grundfos approach to intelligence, water and energy, or search Grundfos research & insights for more learning materials, articles, white papers, videos and much more that benefit your solution.