FAQ

Question: What is Grundfos Distributed Pumping?

Answer:

Grundfos Distributed Pumping solution is the new revolutionary offering for distribution of chilled water in HVAC applications without the need for pressure regulating valves. 

With a distributed pumping solution, you will gain:

  • Up to 50% energy savings on your annual pumping power use by using the worlds’ most energy efficient pumps. 
  • Flow-driven pumping solution that gives you just the right flow to meet your heat load demand.
  • Valve-less design, reducing system pressure and eliminating the need for costly balancing.

Additional information:

Distributed Pumping solutions replace larger centralised pumps and energy-consuming balancing and control valves with smaller intelligent pumps placed on each floor of the building. The result is substantial energy savings and a more comfortable indoor climate.