FAQ

Question: What happens if the pump is operating too far to the right on the curve?

Answer:

When a pump operates too far to the right on the curve, this simply means that the pump is delivering a flow rate greater than that for which it was designed. In other words: The pump is too small for the volume flow needed by the system. Operating the pump in this range may cause damage to the pump and the motor.

The pump must always be operated within the lower and upper flow rate bounds. Ideally, the pump should be operated as close as possible to the point of optimal efficiency in order to ensure a long service life and in order to minimise energy consumption.

Additional information:

Enhance your knowledge

Find out how to get reduced energy consumption, increased comfort and unsurpassed operational reliability for your application. Read our customers' stories about how they benefit from the Grundfos approach to intelligence, water and energy, or search Grundfos research & insights for more learning materials, articles, white papers, videos and much more that benefit your solution.