FAQ

Question: How do I install the underwater cable for submersibles?

Answer:

Before installing the underwater cable on the motor, you need to make sure that the cable plug is clean and dry. For ease of installation, the rubber parts of the cable plug should be coated with a non-conductive silicone paste. The screws that hold the cable in place should be tightened using the following tightening torques:

MS 4000: 2.0 Nm

MS 402: 2.0 Nm

MS 6000: 4.0-5.0 Nm

MMS 6000: 10 Nm

MMS 12000: 15 Nm

Additional information:

Enhance your knowledge

Find out how to get reduced energy consumption, increased comfort and unsurpassed operational reliability for your application. Read our customers' stories about how they benefit from the Grundfos approach to intelligence, water and energy, or search Grundfos research & insights for more learning materials, articles, white papers, videos and much more that benefit your solution.