6 questions Basic

ECADEMY test

62 - The COMFORT Hot Water Recirculation Course

This course test contains 6 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 1 of 6 Basic

How much electricity can be saved on average by using the AUTOADAPT operation mode?

Question 3 of 6 Basic

On which pipe do you mount the pump?

Question 4 of 6 Basic

How high are the potential energy savings you can achieve with Comfort with AUTOADAPT?

Question 5 of 6 Basic

Which of these isn't a major downfall of a pump running round the clock?

Question 6 of 6 Basic

Which of these is NOT one of COMFORT with AUTOADAPT's three operation modes?

Question 6 of 6 Basic

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 62 - The COMFORT Hot Water Recirculation Course

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 62 - The COMFORT Hot Water Recirculation Course test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: How much electricity can be saved on average by using the AUTOADAPT operation mode?
A: 96%
Correct
Q: How do you identify the supply pipe?
A: You let the hot water run and feel which pipe gets warmer
Correct
Q: On which pipe do you mount the pump?
A: The return pipe
Correct
Q: How high are the potential energy savings you can achieve with Comfort with AUTOADAPT?
A: Approximately 48%
Correct
Q: Which of these isn't a major downfall of a pump running round the clock?
A: Increased noise
Correct
Q: Which of these is NOT one of COMFORT with AUTOADAPT's three operation modes?
A: Full Flow