News
Grundfos Unveils New MLE Motor: Setting a New Standard in Pump Technology
16-May-2024
[Lenexa, Kansas, May 1, 2024] – Grundfos, a global leader in advanced pump solutions, is thrilled to announce the release of its latest innovation, the MLE motor series. Engineered to meet the demands of modern industry, this cutting-edge motor showcases a range of features and advancements, including a power output of up to 30 horsepower (HP), an integrated Safe Torque Off (STO) function, Modbus RTU built-in as standard, Bluetooth connectivity for effortless communication with Grundfos GO, and an Ethernet port for seamless access to Cloud and Grundfos GO Link (only available on 20, 25 and 30hp models).
The MLE motor is designed with customer safety and convenience in mind. With its integrated STO function, the motor mitigates the risk of exposure to high pressure or hazardous liquids in open systems, ensuring maximum safety for workers and the environment. Furthermore, the motor offers a variety of connectivity options, enabling seamless communication with Grundfos GO and easy access to Cloud and Grundfos GO Link via the Ethernet port.
"We are excited to introduce the new MLE motor, which builds on our strong tradition of innovation and excellence in motor technology," said Jay Stellmacher, Senior Regional Sales Director for Grundfos Industry Americas. "This latest generation motor is designed to provide our customers with the highest level of safety and connectivity, ensuring maximum convenience and peace of mind."
The MLE motor is not only highly efficient but also environmentally friendly. Its variable speed drive allows users to adjust motor speed to match system demand, resulting in maximum energy savings of up to 30% compared to NEMA premium efficient motors. This significant reduction in energy consumption translates to a reduced carbon footprint, making the motor an eco-conscious choice for customers.
In addition to its advanced safety and connectivity features, the MLE motor boasts easy installation and maintenance, thanks to its user-friendly interface that allows for quick and simple adjustments.
The new MLE motor is available across all verticals, including Multistage, Immersible, Inline, and End-Suction pumps, and is ready for purchase now. Grundfos invites customers to experience the new generation of advanced motor technology, setting new benchmarks for safety, efficiency, and reliability in the industry.
For more information about the MLE motor series, visit grundfos.us.
About Grundfos:
Grundfos is a global leader in advanced pump solutions, dedicated to pioneering technologies that improve the quality of life and contribute to a sustainable future. With over 75 years of experience, Grundfos continues to innovate and set industry standards in pump technology.
Media Contact:
Krystyn DeMasie, Senior Marketing Specialist, kdemasie@grundfos.com