8 questions Intermediate

ECADEMY test

Groundwater Pumping

This course test contains 8 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 1 of 8 Intermediate

What kind of riser pipe is most likely to keep itself free from scaling?

Question 3 of 8 Intermediate

What should the minimum flow past the motor be to ensure sufficient motor cooling?

Question 5 of 8 Intermediate

By-pass control is an efficient way of performance regulating a pump but what is the downside of the process?

Question 8 of 8 Intermediate

In which areas is there a bigger risk of pumping corrosive groundwater?

Question 8 of 8 Intermediate

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the Groundwater Pumping

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the Groundwater Pumping test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: What kind of riser pipe is most likely to keep itself free from scaling?
A: Flex hoses
Correct
Q: What can be done to the well if sand continues to enter a well after the well development has been carried out?
A: The well driller can try to run the pump at its maximum capacity in short periods of time over a couple of days
Correct
Q: What should the minimum flow past the motor be to ensure sufficient motor cooling?
A: 0,15 m/s
Correct
Q: Why is it important to know the water drawdown?
A: The more the drawdown increases during pump operation, the more pressure is required to lift the groundwater to the surface
Correct
Q: By-pass control is an efficient way of performance regulating a pump but what is the downside of the process?
A: Energy is wasted as the pump continues to run at full speed
Correct
Q: Why is it a good idea to make a well where the groundwater level is as high as possible?
A: The shorter the distance is to the water the less expensive it is to make the borehole and subsequently to pump the water to the surface
Correct
Q: What could be the consequences of using an undersized pump in a well?
A: The pump may not be able to deliver the required capacity
Correct
Q: In which areas is there a bigger risk of pumping corrosive groundwater?
A: In coastal areas