Case
Indian Dyeing Company Goes Green with Grundfos Solutions
Topic:
Indian dyeing company goes Green with Grundfos Solutions
Location:
Tirupur
Company:
India Dyeing Pvt Ltd
India Dyeing Pvt ltd, Tirupur is a manufacturer and exporter of Golf Shirts, Polo Shirts, Pigment Dyed Garments and Knitted garments for Men, Women and children. The company also offers trendy Polo shirts and Golf shirts. A variegated product range offers a diverse collection of colors both vibrant and docile and trends that conform to the latest. Contemporary style, varied fashion lines and wide range of designs coupled with superior fabrics that retain their gloss and clarity of textural characteristics.
THE SITUATION
Soft flow dyeing machines are suitable for the processing of both woven as well as knitted fabric. Any fabric, from lightweight silk to suitings can be processed at ease with this dyeing machine. The process can be repeated and reproduced
The Soft Flow dyeing machine has a tank that is to be filled for 20 cycles. In each cycle the tank has to be filled up thrice within the shortest possible time. Depending on the demand, this filling of up of tanks used to take longer time as there was a single pump with a throttle mechanism. It was a challenging task to maintain all the 15 Soft Dyeing Machines according to the demand.
THE SOLUTION
Grundfos believes in Demand Driven Distribution system. Based on the capacity of filling of the tank, Grundfos suggested Hydro 1000 system to take care of the fluctuating demand. The transfer and the pressure boosting of clean water met the demand and the work was smoothly done. In order to optimize pump performance, a variable speed system was installed to fill the tanks faster.
The technical data of the Hydro 1000
Flow rate: max. 1080 m³/h
Head: max. 250 m
Temperature: max 50°C
Operate Pressure: max. 10 bar
THE OUTCOME
With Hydro 1000 there was a trouble free operation of the pumps. The availability of Grundfos spares and the services impressed India Dyeing Pvt Ltd and was deeply appreciated. The performance was satisfactory
Features for Grundfos pumps are listed below –
1. Ease of operation
2. Trouble-free operation
3. Availability of spares and service on time
Have a Grundfos Account?
Login to your Grundfos Account to download the case story today or Register now for free!