Heavy rain, leaking cellar doors, lack of backflow protection or water in the basement. Treat flooding immediately with the Grundfos MULTIBOX.

 

Heavy rain, overflowing rivers, burst pipes – if you must watch helplessly as your own house runs full of water, time is crucial to avoid costly damage.

Early and prudent reaction minimizes major property damage considerably: provided you have the necessary equipment at hand in an emergency. With the MULTIBOX, you can react quickly and decisively in the event of a crisis if part of your property is under water. In addition to the flat-suction UNILIFT CC dirty-water pump, it contains all the necessary hoses and materials for rapid cellar drainage.

Preventive protective measures will become increasingly important in the future. Due to climate change, large-scale weather conditions will settle in one place for longer, which means that more and more areas are exposed to potential flood risks. As a result, infrastructure is overloaded more frequently and surprisingly, floods and unwanted water intrusions. Secure yourself and your property at an early stage in the event of a flooded cellar – with the MULTIBOX as a real flood rescue package, you can tackle any situation decisively.

In this video we will show you how to use the MULTIBOX and the UNILIFT CC correctly for cellar drainage – or alternatively empty your pond or pool.

In an emergency: everything together with the MULTIBOX

The MULTIBOX is specially designed for flood and heavy rain protection. Everything is at hand and in one place, especially in hectic situations. The carrying box contains everything you need to protect your home: an extra-long 15 m pressure hose with stainless steel kink protection, which guarantees maximum pump performance even with sharp turns; an integrated check valve that prevents backflow, and the Grundfos UNILIFT CC water pump with a 10 m cable.

When every second counts

Always ready and ready for immediate use – just what matters with a drainage pump in an emergency. This is exactly what we have achieved with the UNILIFT CC at the heart of our rescue package: Thanks to the multi-sized adapter, the vertical and horizontal connection options and the integrated check valve, there is no need to fumble with connections or desperately look for adapters and accessories when it matters – grab MULTIBOX, connect the pump and save valuable minutes. Fits anytime and anywhere.

Stay well protected with UNILIFT CC

If the basement is flooded, you can prevent major water damage with the right shallow water pump, such as the heart of our MULTIBOX – the UNILIFT CC. With the UNILIFT CC, we rely on a proven concept, and we are constantly developing for more flexibility in connection types, better operability in confined spaces and high reliability even with rough use.

Double outlet

The UNILIFT CC features a double outlet, so it immediately fits on all connections, horizontally or vertically.

Flat suction to less than 3 mm

By simply removing the screen foot, the UNILIFT CC enables flat extraction of up to 3 mm residual water level, so that the floor is wipe dry.

Automatic venting

Automatic venting ensures smooth operation, even in turbulent water inlet or dry pump sump.

Read more about how to handle rainwater flooding

Flooding in houses can lead to serious damage to contents and also lead to the formation of mold. With the right drainage solution, you can stay ahead of these challenges.

Drainage pumps for inside or outside the home

As a rule, domestic wastewater is discharged without additional facilities via a natural slope. It’s only when problems with backwater and flooded cellars occur, appropriate measures must be taken. 
Grundfos offers a wide range of particularly reliable and efficient solutions for all building drainage tasks.

UNILIFT CC

Composite drainage pumps with a free passage of 10 mm for pumping clean, non-aggressive water and slightly contaminated dirty water (grey water).
 

UNILIFT KP

Stainless steel drainage pumps for pumping non-aggressive water and grey water, such as leachate and domestic wastewater with solid particles of maximum 10 mm.

UNILIFT AP

Stainless steel. Clean, non-aggressive, lighter gray wastewater/without faeces. Vertical departure. Variants for respectively 12 mm and 35 mm particles.
 

Become an expert in just a few clicks

Save time in your daily work by improving your skills, your know-how and your business with the online training platform ECADEMY.

Click on a course below to start your training now.