News

Check up on your pump’s health

This is what a large office building in central London did when they replaced obsolete pumps with new, energy-efficient models following a Grundfos onsite check-up. The pumps now operate to meet the actual demand, and the new pumps are delivering a saving 318,000 kWh per year after the estate’s personnel followed through on recommendations they received having undertaken a Grundfos energy check. This has amounted to a massive saving of £30k p.a., a large reduction in CO2 emissions and a short payback period.

Grundfos are typically able to achieve energy savings of 30-60% for customers. By checking up on your pumps and pump solution, this will point the way towards the optimal pump replacement that will deliver the greatest energy savings. In return, you will get reliable operation, less downtime and reduced repair costs. The result: greatly improved system reliability.