6 questions Intermediate

ECADEMY test

8 - Water boosting in commercial buildings

This course test contains 6 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 5 of 6 Intermediate

How is it possible to make sure that an entire system performs at the best efficiency point at all times?

Question 6 of 6 Intermediate

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 8 - Water boosting in commercial buildings

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 8 - Water boosting in commercial buildings test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: What are the benefits of an IE4 motor?
A: Fitted with a frequency drive the motor can adjust its speed to demand to lower energy consumption and wear
Correct
Q: What is the benefit of a booster pump with variable speed
A: The pump automatically adjusts to changes in the water consumption to keep energy usage as low as possible
Correct
Q: What is the purpose of a booster pump?
A: To increase water pressure
Correct
Q: Does a zone divided system require pressure relief valves?
A: No
Correct
Q: How is it possible to make sure that an entire system performs at the best efficiency point at all times?
A: An intelligent controller
Correct
Q: Why are pressure relief valves not required in an intelligently designed boosting solution?
A: There is no excessive pressure in the system