6 questions Intermediate

ECADEMY test

43 - The MAGNA1 Model C circulator pump

This course test contains 6 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 1 of 6 Intermediate

How many levels are there in each of the three pre-defined control functions?

Question 2 of 6 Intermediate

What do you call a feature where one pump acts as a redundant backup to the other?

Question 3 of 6 Intermediate

What is the maximum pressure level that MAGNA1 Model C can provide?

Question 4 of 6 Intermediate

Which of these can’t you do in Grundfos GO?

Question 6 of 6 Intermediate

How do you connect the pump with Grundfos GO Remote?

Question 6 of 6 Intermediate

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 43 - The MAGNA1 Model C circulator pump

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 43 - The MAGNA1 Model C circulator pump test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: How many levels are there in each of the three pre-defined control functions?
A: Three
Correct
Q: What do you call a feature where one pump acts as a redundant backup to the other?
A: Duty/standby mode
Correct
Q: What is the maximum pressure level that MAGNA1 Model C can provide?
A: 16 bar
Correct
Q: Which of these can’t you do in Grundfos GO?
A: Set control function
Correct
Q: Which control function is MAGNA1 factory-set to?
A: Intermediate proportional pressure function
Correct
Q: How do you connect the pump with Grundfos GO Remote?
A: Via an infra-red connection