News
DBS SQ Campaign in Central Java
20-Nov-2014
DBS Team of PT Grundfos Pompa, are back with their successful in re-launching products of SQ Submersible Pump for the fifth time. This time, the event was held in Central Java, and divided into three sessions, first on 28 October in Semarang, 30 October in Solo and the last part in Yogyakarta on 31 October 2014.
"The advantages of SQ pump is capable of operating from a voltage of 150 volts up to 315 volts, these pumps also have dry running protection, plus, lightweight size with a diameter only 3 inches, made of high quality stainless steel which is resistant to corrosion, and really easy to install ". said F.Chandradinata as DBS Business Unit Manager while giving a speech.
The event was quite successful. This proven by many guests who ordered this product during the event until the number reached up to 155 units, and, for your information, this number are continues to increase, even after the event is over.
This SQ Pump Re-launching Event in Central Java is a continuation of the re-launching SQ Submersible pumps that had previously been held in Bandung, Jakarta, Bali, and Surabaya. Also we, DBS team, would like to say thank you to all of you who have participated in this event.