6 questions Basic

ECADEMY test

15 - Pump sizing

This course test contains 6 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 1 of 6 Basic

How many hours will a correctly sized pump run a day to meet the demand?

Question 3 of 6 Basic

Which of the following parameters is determined by the amount of water to be applied during the peak period?

Question 5 of 6 Basic

What is the limit of sand in well water as recommended by US EPA and National Water Works Association for flood irrigation?

Question 6 of 6 Basic

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 15 - Pump sizing

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 15 - Pump sizing test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: How many hours will a correctly sized pump run a day to meet the demand?
A: 12-18 hours
Correct
Q: What are the two factors that should be ensured when the total head for a ground water pump is calculated?
A: There is no suction lift. Instead there is static water table and the drawdown has to be added to the elevation lift.
Correct
Q: Which of the following parameters is determined by the amount of water to be applied during the peak period?
A: The minimum size of the pump
Correct
Q: Which of the following options is true about a centrifugal pump?
A: If the pump is pumping at a lower flow, it delivers a higher head.
Correct
Q: What is the limit of sand in well water as recommended by US EPA and National Water Works Association for flood irrigation?
A: 15ppm
Correct
Q: How do we calculate head requirement from the pump?
A: Elevation lift + static water level + drawdown in the well + pressure head of the application device + friction loss in the pipes