8 questions Advanced

ECADEMY test

29 - Introduction to temperature control

This course test contains 8 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 1 of 8 Advanced

What is the expected payback time of an investment in system optimisation?

Question 2 of 8 Advanced

How do you prevent pumps from malfunctioning when transporting hot water with a temperature of well above 120C°?

Question 4 of 8 Advanced

What is the ratio between the capital investment and running costs of a temperature control system?

Question 7 of 8 Advanced

How high is the suction lift of the self-priming CM pump?

Question 8 of 8 Advanced

Which component is often ‘the weakest link’ in centrifugal pumps?

Question 8 of 8 Advanced

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 29 - Introduction to temperature control

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 29 - Introduction to temperature control test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: What is the expected payback time of an investment in system optimisation?
A: 1-5 years
Correct
Q: How do you prevent pumps from malfunctioning when transporting hot water with a temperature of well above 120C°?
A: Equip the pump with double-shaft seals or air-cooled top.
Correct
Q: What is the most efficient and simple way of controlling heating, cooling and refrigeration systems?
A: Intelligent pumps equipped with temperature sensors that measure the outlet temperature and signal the pump to regulate its flow accordingly – without the use of valves.
Correct
Q: What is the ratio between the capital investment and running costs of a temperature control system?
A: 1:20
Correct
Q: Why is ammonia an efficient coolant?
A: Ammonia is able to absorb large amount of heat when it evaporates.
Correct
Q: Which load profile will benefit the most from a demand driven control system?
A: Low flow rate with relatively few peak periods during the day.
Correct
Q: How high is the suction lift of the self-priming CM pump?
A: Up to 8 metres
Correct
Q: Which component is often ‘the weakest link’ in centrifugal pumps?
A: Shaft seal