Article

Lack of water pressure or noisy boosting system?

Difficulties rinsing out the shampoo, fluctuating shower temperatures, slow filling toilets, noise from water pipes or pump inside or outside of the home. Over time, these irritations can compromise comfort in the home. Luckily, there’s a solution to improving the domestic water supply system – The SCALA Pumps.

Watch the video and see how you make better domestic pressure boosting systems.

Lack of water pressure?

Insufficient water pressure can extend toilet tank refilling times, resulting in longer waiting time before flushing. A lack of water pressure can also cause temperatures to become unstable and fluctuate between scalding hot and freezing cold in the shower. Asides from being uncomfortable to live with, insufficient water pressure can cause problems when running domestic appliances like washing machines or dishwashers.

Watch the video and see how you make better domestic pressure boosting systems.


Identifying the cause

If your boosting system is supplied with water from a city water mains or shallow wells, you might experience fluctuations or even no pressure coming from the city water mains. If your water supply comes from a rooftop tank or a break tank elevated from either ground level or below ground level, the pressure might not be sufficient to supply all taps and appliances with adequate levels of water pressure. In this case, you will need a pressure booster. Otherwise, you will not get any water coming out of the taps.

Noisy booster system?

Noise from water pipes or the booster pump can be annoying for you and your neighbors. In most cases, noisy pipes indicate problems in the water supply system. Since noise is easily transmitted via structures and components in the water supply system, it can be difficult to identify the source of the issue.  However, the most common reason is due to poor pump technology or poor pump control. Systems with older centrifugal pumps that use fan-cooled motors, for instance, can generate vibrations throughout the system, resulting in more noise. Inefficient pumps that run constantly, even when there is no water being used, or poorly installed booster pumps that are not secured to the floor, can cause vibrations and noise in the system.

Watch the video and see how you make better domestic pressure boosting systems.

Enhance comfort in the home with a Grundfos booster solution

The Grundfos SCALA Pump family integrates all components into one compact boosting device that includes a pump, tank, sensor and non-return valve. 

Equipped with cutting edge technology, the SCALA1 and SCALA2 use intelligent water-cooling technology to reduce noise and vibration. During typical use, the SCALA1 omits > 55 dB(A) while the SCALA2 omits < 47 dB(A). A decrease in sound level of 6 dB(A) will actually appear as the noise has halved in loudness. For comparison, most dishwashers omit around 46-60 dB during typical use. 

For ultimate comfort and intelligent features that adjust performance to the home, choose SCALA2, our premium pump that keeps noise to a minimum and gives perfect water pressure.

 

Source

Want to learn more?

We have a dedicated learning track that will give you hands-on learning about domestic water pressure boosting and our solutions. If you complete a learning track you will be rewarded with a badge.

Sign up for the latest news on products, tools, training and events