6 questions Basic

ECADEMY test

15 - Pump sizing

This course test contains 6 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 4 of 6 Basic

Identify the factors that are not considered for calculating the total pump head requirements?

Question 5 of 6 Basic

What is the limit of sand in well water as recommended by US EPA and National Water Works Association for flood irrigation?

Question 6 of 6 Basic

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 15 - Pump sizing

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 15 - Pump sizing test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: What determines the minimum flow of a pump?
A: The amount of water that needs to be applied to the crops during peak periods.
Correct
Q: Identify which of the following sentences are true:
A: The drawdown is the difference between the static and the dynamic water level.
Correct
Q: Which of the following options is true about a centrifugal pump?
A: If the pump is pumping at a lower flow, it delivers a higher head.
Correct
Q: Identify the factors that are not considered for calculating the total pump head requirements?
A: Pump flow
Correct
Q: What is the limit of sand in well water as recommended by US EPA and National Water Works Association for flood irrigation?
A: 15ppm
Correct
Q: How do we calculate head requirement from the pump?
A: Elevation lift + static water level + drawdown in the well + pressure head of the application device + friction loss in the pipes