6 questions Basic

ECADEMY test

14 - Motors and motor protection

This course test contains 6 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 1 of 6 Basic

The slots located in the inner diameter of a stator have:

Question 3 of 6 Basic

Which of the following causes slow temperature increase in the motor winding?

Question 4 of 6 Basic

Which formula will you use to calculate motor efficiency if the motor size is listed in hp?

Question 5 of 6 Basic

By using the Grundfos MP204 protection device and a CIU communication unit, the monitored data can be:

Question 6 of 6 Basic

Which of the following things does a built-in protection device normally sense and protect against:

Question 6 of 6 Basic

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 14 - Motors and motor protection

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 14 - Motors and motor protection test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: The slots located in the inner diameter of a stator have:
A: Copper wires
Correct
Q: Which of the following statements is true about pump protection devices?
A: Motor protection offers monitoring of the motor and protection.
Correct
Q: Which of the following causes slow temperature increase in the motor winding?
A: Frequent starts with high inertia load
Correct
Q: Which formula will you use to calculate motor efficiency if the motor size is listed in hp?
A: (P2× 0.746/P1) × 100%
Correct
Q: By using the Grundfos MP204 protection device and a CIU communication unit, the monitored data can be:
A: Transmitted to the central controller
Correct
Q: Which of the following things does a built-in protection device normally sense and protect against:
A: Temperature