8 questions Intermediate

ECADEMY test

39 - The ALPHA2 circulator pump and easy balancing with the GO Balance app

This course test contains 8 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 2 of 8 Intermediate

What is the primary advantage of using the ALPHA Reader and the Grundfos GO Balance app in balancing jobs in one-family homes?

Question 3 of 8 Intermediate

AUTOADAPT is the most efficient choice of control mode in what percentage of all systems?

Question 5 of 8 Intermediate

If you need to balance both the radiator and the underfloor heating system in a combined system, how many ALPHA2 pumps must be installed?

Question 6 of 8 Intermediate

Is it possible to generate documentation and email or print it directly from the app?

Question 7 of 8 Intermediate

What are constant pressure control modes mainly used for with an ALPHA2?

Question 8 of 8 Intermediate

Which control modes should never be used in systems with TRVs?

Question 8 of 8 Intermediate

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 39 - The ALPHA2 circulator pump and easy balancing with the GO Balance app

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 39 - The ALPHA2 circulator pump and easy balancing with the GO Balance app test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: What is the Grundfos GO Balance app?
A: An intuitive step-by-step guide for balancing processes
Correct
Q: What is the primary advantage of using the ALPHA Reader and the Grundfos GO Balance app in balancing jobs in one-family homes?
A: Balancing of all radiators can be completed in less than two hours
Correct
Q: AUTOADAPT is the most efficient choice of control mode in what percentage of all systems?
A: More than 80%
Correct
Q: When balancing a combined radiator and underfloor heating system you should always:
A: Balance all radiators in the system first
Correct
Q: If you need to balance both the radiator and the underfloor heating system in a combined system, how many ALPHA2 pumps must be installed?
A: One ALPHA2 that runs the radiator system and one ALPHA2 that runs the underfloor heating system
Correct
Q: Is it possible to generate documentation and email or print it directly from the app?
A: Yes
Correct
Q: What are constant pressure control modes mainly used for with an ALPHA2?
A: Underfloor Heating
Correct
Q: Which control modes should never be used in systems with TRVs?
A: Fixed speed modes