Artikkel

Energy efficiency holds the key to more sustainable commercial buildings

We urgently need to change the way we build and operate our buildings. Because buildings account for a significant portion of global energy consumption – in fact, most buildings use between 20 and 50% more energy than necessary. And that’s even factoring in new constructions or newly renovated buildings.

But we believe it’s possible to change this – and that there’s still massive potential to save energy in buildings. It all starts with intelligent solutions that enable more energy-efficient HVAC and water systems. 

Energy efficiency is crucial for creating a sustainable future

As our CEO Bent Jensen puts it, we can only achieve a green energy transition if we reduce our energy use. And according to the International Energy Agency, energy efficiency is the first fuel in the fight against climate change.

The solutions we need are already available today. Now we just need to start implementing them at scale in buildings all around the world. 

Most buildings, including new constructions, use 20-50% more energy than necessary.

Grundfos is the first water solution company in the world to receive a validated SBTi target.

Driving real progress through collaboration

We have a strong belief in the potential of energy efficiency – and we’re proud to have made progress, becoming the first water solution company in the world to receive a validated SBTi target.

We are also working to phase out traditional fixed-speed pumps, moving towards energy-efficient e-pumps with a frequency converter that help ensure the pump only runs when needed. 

This is just one of the initiatives that make up our innovation roadmap – but we won’t be able to do it on our own. That’s why we want to bring together property owners, designers, consultants, contractors, operators and suppliers.

Watch the film to find out how we can work together to eliminate a substantial part of the energy consumed by water and HVAC systems in many buildings – without anybody ever noticing.

Get in contact today to book an energy check. We work fast, and you’ll often have the final report on your table after only two weeks. Based on this, we can offer a follow-up meeting to discuss the results and assess your options for further energy optimisation.