FAQ
Question: Why is the heating system making noise?
Answer:
Possible cause of the fault
The flow rate is too high
This can be resolved by setting the pump to a setting other than "AutoAdapt"
Note the pump setting that appears on the display.
Then use Button 5 to switch the pump to "AutoAdapt". (for MAGNA, use Button 3)
If the supply of heat is sufficient at this point, leave it at this setting.
If the supply of heat is not sufficient, restore the previous setting using Button 5 (for MAGNA use Button 3), and then call your installer.
The air in the system.
Remedy
These faults can only be remedied by a specialist company.
Additional information:
Enhance your knowledge
Find out how to get reduced energy consumption, increased comfort and unsurpassed operational reliability for your application. Read our customers' stories to learn how they benefit from the Grundfos approach to intelligence, water and energy. You can also search Grundfos research and insights for more learning materials, articles, white papers, videos and much more content to inform your solution.