FAQ
Question: What is the role of the bypass lines and how should these be routed?
Answer:
In order to ensure adequate cooling and lubrication of the pump, there must be sufficient volume flow through the pump. Inadequate cooling and lubrication leads to overheating, bearing wear, friction between the sealing faces, leaks at the shaft seal, all of which will lead to pump malfunctions or failures. This is why a bypass line needs to be installed if there is a risk that the pump cannot be operated at the necessary minimum flow rate.
The bypass line is to be drawn from the pump's vent port or the discharge pipe's vent port, either back to the suction side (if possible) or into a tank, in order to ensure sufficient cooling by the pumped medium. On return, it must be possible for the pumped medium to cool down before it is fed back into the pump in order to avoid overheating the pump. For this reason, the bypass line must never be connected directly to the pump's suction port. The bypass line has been configured correctly if the minimum flow rate requirements for the respective pump as specified in the operating instructions have been fulfilled. At full load, the volume flowing through the system and the bypass may not exceed the maximum flow rate delivered by the pump.
Additional information:
Enhance your knowledge
Find out how to get reduced energy consumption, increased comfort and unsurpassed operational reliability for your application. Read our customers' stories to learn how they benefit from the Grundfos approach to intelligence, water and energy. You can also search Grundfos research and insights for more learning materials, articles, white papers, videos and much more content to inform your solution.