FAQ
Question: What is Grundfos Distributed Pumping?
Answer:
Grundfos Distributed Pumping solution is the new revolutionary offering for distribution of chilled water in HVAC applications without the need for pressure regulating valves.
With a Distributed Pumping solution, you will gain:
- Up to 50% energy savings on your annual pumping power use by using the worlds’ most energy efficient pumps.
- Flow-driven pumping solution that gives you just the right flow to meet your heat load demand.
- Valve-less design, reducing system pressure and eliminating the need for costly balancing.
Additional information:
Distributed Pumping solutions replace larger centralized pumps and energy-consuming balancing and control valves with smaller intelligent pumps placed on each floor of the building. The result is substantial energy savings and a more comfortable indoor climate.