How to save up to 40% in energy consumption by using Hydro MPC BoosterpaQ’ s advanced motor and control technology
The purpose of this training is to understand the impact of the new Permanent Magnet (ECM) MLE motor has for Hydro MPC BoosterpaQ and to review many of the energy saving control features in the CU352. The new MLE motor along with the control functionality in the CU352 controller, make energy savings up to 40% possible compared to competition
Webinar overview
01-08-2022
01:00 - 2:00 CET
English