Research And Insight
Vortex impeller
The vortex impeller creates a revolving mass of water which forms a whirlpool. A whirlpool is a funnel shaped opening is created downward from the water surface. It can be developed by water flowing out of a small opening in the bottom of a basin, a reservoir or by a pump. Impellers creating this Vortex are called vortex impellers.
The benefit of a vortex impeller over a channel impeller is the minimized risk of clogging. A vortex impeller is also a better choice when the pumped liquid has a high content of sand. The efficiency of a pump with a vortex impeller is typically lower than a pump with a channel impeller.
Grundfos supplies submersible and dry-installed wastewater pumps with vortex impellers with a low risk for clogging.