8 questions Intermediate

ECADEMY test

3 - Wastewater

This course test contains 8 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 3 of 8 Intermediate

Who has the financial responsibility in the case of flooding in most countries?

Question 4 of 8 Intermediate

Which method of backflow prevention has the following disadvantages: Highly sensitive to sand and solid objects in the water. In a backflow situation, it is not possible to use the sanitary facilities that are connected to this device. Storm water drains cannot be connected to this device. The device is not 100% safe and should be used only to protect secondary rooms with no vital technical installations.

Question 6 of 8 Intermediate

Which method of backflow prevention has the following advantages: Offers maximum backflow and flooding protection: Is not sensitive to fat, grease, sands and solids in the water. Makes it possible to use sanitary facilities in case of backflow. Offers protection for paved areas. Can be connected to buildings’ storm water drains.

Question 8 of 8 Intermediate

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 3 - Wastewater

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 3 - Wastewater test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: Why is the life cycle cost of the pressurised wastewater system low?
A: The initial cost of the lifting station is lower compared with a pit and there are no gravitation pipes outside the building
Correct
Q: Of the three anti-flooding systems, why is the lifting station the superior system?
A: It is pre-assembled and its location inside the building makes it easily accessible for service. Furthermore, it offers maximum backflow and flooding protection
Correct
Q: Who has the financial responsibility in the case of flooding in most countries?
A: The building owner and the building designers
Correct
Q: Which method of backflow prevention has the following disadvantages: Highly sensitive to sand and solid objects in the water. In a backflow situation, it is not possible to use the sanitary facilities that are connected to this device. Storm water drains cannot be connected to this device. The device is not 100% safe and should be used only to protect secondary rooms with no vital technical installations.
A: Anti-flooding valves
Correct
Q: What is grey wastewater?
A: Water, which is discharged from showers, sinks, washing machines, canteen kitchens etc.
Correct
Q: Which method of backflow prevention has the following advantages: Offers maximum backflow and flooding protection: Is not sensitive to fat, grease, sands and solids in the water. Makes it possible to use sanitary facilities in case of backflow. Offers protection for paved areas. Can be connected to buildings’ storm water drains.
A: Pumping stations
Correct
Q: Under which circumstances should you consider a pressurised wastewater system rather than a gravitation system
A: When there is a long distance between the building and the sewer main, when the sewer main is up-hill or when there are obstacles between the building and the sewer main.
Correct
Q: What are the disadvantages of the traditional gravitation system?
A: Many gravitation pipes have to be installed outside the building and a great deal of excavation work is needed.