4 questions Intermediate

ECADEMY test

1 - Life Cycle Cost

This course test contains 4 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 1 of 4 Intermediate

Which control mode is used in variable flow systems where the pressure requirement is the same regardless of flow?

Question 3 of 4 Intermediate

What is the approximate energy savings achieved by using the proportional pressure control mode with a quadratic curve setting?

Question 4 of 4 Intermediate

With which setting is there no need to install pressure sensors far away from the pump?

Question 4 of 4 Intermediate

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the 1 - Life Cycle Cost

Achieved badges:

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Continue training Go to MyECADEMY

Sorry. You did not pass the 1 - Life Cycle Cost test this time

How would you rate this course?

You are welcome to add your rating of this course. Remember that you have to be logged in before you take the test to be able to give your rating.

Correct
Q: Which control mode is used in variable flow systems where the pressure requirement is the same regardless of flow?
A: Constant differential pressure mode
Correct
Q: In the imaginary scenario, which system is the most expensive?
A: The variable flow system with a constant speed pump
Correct
Q: What is the approximate energy savings achieved by using the proportional pressure control mode with a quadratic curve setting?
A: At least 15%
Correct
Q: With which setting is there no need to install pressure sensors far away from the pump?
A: "Quadratic" curve