FAQ

Question: Can the pump be operated using a frequency converter?

Answer:

Grundfos offers numerous speed-controlled pumps that are referred to as ‘E-pumps’ and which come equipped with Grundfos MGE motors with an integrated frequency converter. The manufacturing costs and material inputs are lower compared to pump solutions with external frequency converters. In addition, technical issues that may arise in connection with external frequency converters are avoided.

Finally, MGE motors have numerous additional features and advantages. In the event that no E-pump is available for a specific application, it is generally possible to operate the three-phase industrial motors offered by Grundfos via an external frequency converter. The technical information set out in the operating instructions and datasheet should be referred to in each individual case. 

All Grundfos submersible well motors can be operated using a frequency converter.  However, the setup can vary from one type of submersible pump to another.

SQE, all sizes uses a built-in frequency converter working with CU301 Controller.

SP, all sizes, uses an external frequency converter, sold separately.

SPE, all sizes, requires an external frequency converter to start the motor, sold separately.

Additional information:

Enhance your knowledge

Find out how to get reduced energy consumption, increased comfort and unsurpassed operational reliability for your application. Read our customers' stories about how they benefit from the Grundfos approach to intelligence, water and energy, or search Grundfos research & insights for more learning materials, articles, white papers, videos and much more that benefit your solution.